vl Control Effort

Index.Sub  6044.0H
Data Type Integer16
Access Read Only
PDO Mappable TX_PDO (1)
Unit User-defined velocity unit

Range

Integer16

Default Value No
Store Supported No
Description

This object is used for ‘Velocity mode (vl)’ and is the velocity at the motor spindle or load (without closed loop control this value reads the vl Velocity Demand. Positive values shall indicate forward direction and negative values shall indicate backward direction.

 The User-defined velocity unit is converted to the revolution per minute (rpm) with vl Dimension Factor (numerator):

                Velocity [user-defined units] x vl Dimension Factor (numerator) = Velocity [rpm]

        The ‘device internal velocity unit’ is ‘rpm’ [revs/min].

Notes

(1)Available with firmware V00r74 or superior.